AXIS#.SAFEPARAM.SSM_#.VELUPPERLIMIT

Description

Indicates the velocity upper limit of the Safe Speed Monitor (SSM) function.

 

This is n_UL_SSM in the following diagram:

Context

For complete SSM information refer to SSM (Safe Speed Monitor).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

[-2^31+1, 2^31-1]
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
AXIS1.SAFEPARAM.SSM_1.VELUPPERLIMIT

315fh

03h

Signed32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSM_2.VELUPPERLIMIT

3160h

03h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSM_1.VELUPPERLIMIT

325fh

03h

Signed32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSM_2.VELUPPERLIMIT

3260h

03h

Signed32

-

-

Read/Write

No